==============================================================
2v0p1
==============================================================

Added Features
 * General improvements for CLI commands.

Addressed issues:
 * None


==============================================================
2v0p0
==============================================================

Added Features:
 * Added WinUSB support
     The driver mode will change to WinUSB automatically after the update.
     This will cause the USB PID to change, which may cause issues in special setups relying on the PID.
     For Windows 7 and earlier: Please install the latest SEGGER J-Link software pack
     with the "Legacy drivers" option enabled before installing this update.
     If needed, the mode can be changed back to SEGGER using either one of:
     - Simplicity Commander: "commander adapter drivermode" or GUI
     - Admin console: The "sys drivermode" command.
     - SEGGER J-Link Configurator
 * Enabled PCODE and HSS support

Addressed issues:
 * None


==============================================================
1v6p1
==============================================================

Added Features:
 * Support for erasing entire flash when erasing FGPA flash from PC tools

Addressed issues:
 * Fixed issue where mainboard needed to be power cycled after flashing the FPGA


==============================================================
1v6p0
==============================================================

Added Features:
 * Added command to restore default configuration - "sys restore"

Addressed issues:
 * Fixed potential for corrupting configuration
 * Identification of boards could fail intermittently
 * Improved resistance against "garbage" UART bytes when VCOM is disabled
 * Concurrent use of RTT and VCOM could cause data loss on the VCOM channel.


==============================================================
0v9p2
==============================================================

Fixed production test issue


==============================================================
0v9p1
==============================================================

Fixed production test issue


==============================================================
0v9p0
==============================================================

Initial version